Bootloader not jumping to application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader not jumping to application

981 Views
mayur1in
Contributor I

Hello,

Below are my bootloader and application code sequences.

Bootloader steps:

  1. Initialize the BSP, Clock and required peripherals.
  2. Stay in bootloader for BLE connection.
  3. After connection successful, start receiving application binary.
  4. Check CRC if CRC correct then, Erase all sectors for application, write received application binary using SPI driver in to 16Mb ext. flash in to dedicated memory area. (Please see the Bootloader and Application memory address details below.)
  5. After successful written, read back from ext. flash and confirm the CRC.
  6. If CRC matches -> Disable IRQ, Disable peripherals, Initialize SP and PC to application and Jump to Application vector address.

So I have assigned 1 Mb of memory of ext. flash for bootloader i.e. 0x60000000 size 0x100000

And prepare the application binary using keil IDE with 3 Mb space allocated i.e. 0x60100000   Size 0x300000

So I'm initializing the SP, PC and suggesting bootloader to jump on below address of application Vectors

 __Vectors    0x60102000   Number      1024  startup_mimxrt1062.o(.isr_vector)

When I'm flashing my bootloader and application with JTAG ULINKPRO debugger both are working fine.

When I'm trying to update firmware using BLE(By following above Bootloader steps) it's not jumping to application and stuck in BL itself.

I have toggled 2 different LED's i.e.

LED1 Blinks - When I'm in bootloader.

LED2 Blinks - When I'm in application.

 

 

 

0 Kudos
Reply
1 Reply

917 Views
Sam_Gao
NXP Employee
NXP Employee

Hi,

Based on your description, it seems that you can successfully flash your bootloader and application using the debugger, but you are unable to update the firmware via BLE.

Please ensure that your BLE firmware is actually flashed to the correct address and that the firmware itself does not have any issues causing it to get stuck, you can check with trace log with firmware vesion number or timestamp. 

0 Kudos
Reply