Boot from SD Card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot from SD Card

1,512 Views
abady1000
Contributor III

Hello,

I use NXP RT1170, my application is big, I use almost the whole OC RAM (OC1 + OC2 + ECC1 + ECC2), I sue also the other RAM Segments (DTC, ITC, SDRAM)

 

My application is linked to RAM, and when I upload application it uploads every segment into the correct palce it should be in.

I want now to build a bootable image form SD Card, how to do so?

My idea is to modify linker script manually and make all sections uploaded to SDRAM, then in boot CPU put every section in its correct place using Linker Load/Execute address.

 

Is this doable? is there other better means to achieve this?


BTW, when I use Secure Provisioning tool I get this error message after selecting my axf file:
ERROR: The selected image size 540234688 is greater than the selected boot memory size 67108864.

0 Kudos
Reply
3 Replies

1,479 Views
mayliu1
NXP Employee
NXP Employee

Hi @abady1000 ,

Thank you so much for your interest in our products and for using our community.

I suggest you can refer to this link.

RT1050 SDRAM app code boot from SDcard burn with 3 tools - NXP Community

 This document is about the RT series app running on the external SDRAM, but boot from SD card. 

Wish it helps you.
If you still have question about it, please kindly let me know.

Wish you a nice day!

Best Regards
MayLiu

1,281 Views
abady1000
Contributor III
Thank you, it is a great help.
0 Kudos
Reply

1,262 Views
mayliu1
NXP Employee
NXP Employee

You are welcome, and thanks for your reply.

If this post answers your question, please accept it as  solution.

If you meet any issue in the future, welcome to create the new question post.

0 Kudos
Reply