Boot from NAND Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,967件の閲覧回数
Ankush_9881
Contributor II

Hello All,

 I am working on the custom board of iMXRT1176. We are exploring with the NAND memory and have some query for the same.

1. As existing memory is NOR Flash and XIP is there but in case of Serial NAND Flash it is not possible! Am i right ?

2. If XIP is not possible then for Serial NAND Flash , need to copy the code from NAND flash to SDRAM and run from there. Is ROM boot is capable of doing same ?

3. If the ROM Boot is not capable , how do the same ?

Thanks in Advance

Ankush

0 件の賞賛
返信
1 解決策
2,935件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @Ankush_9881 ,

1. Yes, NAND flash doesn't support XIP because it doesn't support random read.

2. Yes, the code in NAND flash must be read to RAM before executing. ROM bootloader is capable to do so.

3. Please see the 10.6.2 section in reference manual.

 

Regards,

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,936件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @Ankush_9881 ,

1. Yes, NAND flash doesn't support XIP because it doesn't support random read.

2. Yes, the code in NAND flash must be read to RAM before executing. ROM bootloader is capable to do so.

3. Please see the 10.6.2 section in reference manual.

 

Regards,

Jing

0 件の賞賛
返信