AN12781 where is nn_quantizer.py ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AN12781 where is nn_quantizer.py ?

1,353 次查看
mtx512
Contributor V

in AN12781 it mentions:

It is recommended to use the nn_quantizer.py python script available with this document in the /Scripts folder.

Which /Scripts it is referring to too as there is not attached source code ?

 

 

 

0 项奖励
回复
1 回复

1,335 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, please check the attachment.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复