16: Target error from status-poll

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

16: Target error from status-poll

Jump to solution
2,310 Views
anthonygarza
Contributor I

16: Target error from status-poll Hardware Transfer Error Debugging context: evkbimxrt1050_freertos_hello LinkServer Debug


I get the above error when debugging a test project. It happens maybe 1 minute after I start debugging and all it is the rtos example renamed. 

This should work yet it is not. 

I start the example connect putty to the com port and it debugs fine the output goes out. But while it is supposed to be suspended it pops this error after a minute or so. 

0 Kudos
Reply
1 Solution
2,299 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to try the below steps to recover the board.
1) Set the SW7 to Serial Downloader.
2) Power on the board, debug the demo project.
3) After that, power off and recover the SW7 to the previous set, then power on again.
4) Give a debug again.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,300 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to try the below steps to recover the board.
1) Set the SW7 to Serial Downloader.
2) Power on the board, debug the demo project.
3) After that, power off and recover the SW7 to the previous set, then power on again.
4) Give a debug again.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply