zImage and device tree in /boot directory of rootfs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

zImage and device tree in /boot directory of rootfs

4,517件の閲覧回数
sebastiaanlaga
Contributor I

Hi All

I am working on QP sabre board.

I really want to have the zImage and device tree file in the /boot directory of my rootfs.

I have already my own layer with linux-imx_*.bbappend file and added

do_install_append() {

   cp arch/{$ARCH}/boot/zImage ${D}/boot/

   cp arch/{$ARCH}/boot/dts/*.dtb ${D}/boot/

}

But yocto complains about: "Please set FILES such that these items are packaged".

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,736件の閲覧回数
steveschefter
Contributor III

Old, but in case anyone else ends up here from a Google search...
Add:
IMAGE_INSTALL_append = " kernel kernel-devicetree"
to your machine .conf file.

3,668件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Sebastian,

please check following thread: How to include any files in rootfs with YOCTO 


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信