yocto toolchains compile optee_example code ,ModuleNotFoundError: No module named 'Crypto'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

yocto toolchains compile optee_example code ,ModuleNotFoundError: No module named 'Crypto'

Jump to solution
4,094 Views
gonewithwind-peter
Senior Contributor I

yocto toolchains compile optee_example code ,ModuleNotFoundError: No module named 'Crypto'

Hi all,

I am playing imx8qm -iwave board.

I use yocto toolchains to cross compile optee_example code,

error happened:

from Crypto.Signature import PKCS1_v1_5

ModuleNotFoundError: No module named 'Crypto'

but I find in toolchain folder, the Crypto folder is there: 

./sysroots/aarch64-poky-linux/usr/lib/python3.7/site-packages/Crypto

It seems the compiler can not find it ?

I have added :

IMAGE_INSTALL_append +=" python3-pycryptodome " in local.conf

any help?

 

Thank you.

 

error:

aarch64-poky-linux-gcc  -fstack-protector-strong  -D_FORTIFY_SOURCE=2 -Wformat -Wformat-security -Werror=format-security --sysroot=/opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux -o optee_example_aes main.o -lteec -L/opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr//lib

make[1]: Leaving directory '/opt/oe/iw/iw-5.4.24/optee_examples/aes/host'

make -C ta CROSS_COMPILE="aarch64-poky-linux-" LDFLAGS=""

make[1]: Entering directory '/opt/oe/iw/iw-5.4.24/optee_examples/aes/ta'

  CC      aes_ta.o

  CC      user_ta_header.o

  CPP     ta.lds

  LD      5dbac793-f574-4871-8ad3-04331ec17f24.elf

  OBJDUMP 5dbac793-f574-4871-8ad3-04331ec17f24.dmp

  OBJCOPY 5dbac793-f574-4871-8ad3-04331ec17f24.stripped.elf

  SIGN    5dbac793-f574-4871-8ad3-04331ec17f24.ta

Traceback (most recent call last):

  File "/usr/local/optee/sysroots/aarch64-poky-linux/usr/include/optee/export-user_ta_arm64//scripts/sign.py", line 78, in <module>

    main()

  File "/usr/local/optee/sysroots/aarch64-poky-linux/usr/include/optee/export-user_ta_arm64//scripts/sign.py", line 31, in main

    from Crypto.Signature import PKCS1_v1_5

ModuleNotFoundError: No module named 'Crypto'

/usr/local/optee/sysroots/aarch64-poky-linux/usr/include/optee/export-user_ta_arm64/mk/link.mk:60: recipe for target '5dbac793-f574-4871-8ad3-04331ec17f24.ta' failed

make[1]: *** [5dbac793-f574-4871-8ad3-04331ec17f24.ta] Error 1

make[1]: Leaving directory '/opt/oe/iw/iw-5.4.24/optee_examples/aes/ta'

Makefile:9: recipe for target 'all' failed

make: *** [all] Error 2

0 Kudos
Reply
1 Solution
4,089 Views
gonewithwind-peter
Senior Contributor I

finally, I have found the solutions. I did it 2 years ago for imx7 board. I remember again.
do not need to modify the recipe.
the toolchain does not include the Crypto package
just manually copy Crypto to toolchain(I do not know how to modify somewhere in the compilation process to copy directly to make it, if someone knows how to do .please tell me ,thank you)

sudo cp -r /home/rnd2/work/maaxboard/zeus/imx-yocto-bsp/maaxboard/build/tmp/sysroots-components/x86_64/python3-pycrypto-native/usr/lib/python3.7/site-packages/Crypto /opt/fsl-imx-wayland-lite/5.4-zeus/sysroots/x86_64-pokysdk-linux/usr/lib/python3.7/site-packages/.

 

 

 

I have found the solution.

please install pycryptodome==3.7 on host opensuse mechine:

pip install pycryptodome==3.7
----
Before I played the old board maaxboard, the python is 2.6, but now it's 3.7. so need to install it.
sometimes ,I am confuse that the pycryptodome should be install in yocto toolcains (DEPENDS += "python3-pycryptodome-native python3-pyelftools-native") or in host machine.

I can find DEPENDS += "python3-pycryptodome-native python3-pyelftools-native" in optee_os.bb file,
so I installed my toolchains in my another ubuntu 18.or host machine. the compilation is passed ! so I thought the error was not in toolchain itself. it should be in host machine.
so I installed : pip install pycryptodome==3.7 on opensuse host. solved it!

View solution in original post

0 Kudos
Reply
2 Replies
4,090 Views
gonewithwind-peter
Senior Contributor I

finally, I have found the solutions. I did it 2 years ago for imx7 board. I remember again.
do not need to modify the recipe.
the toolchain does not include the Crypto package
just manually copy Crypto to toolchain(I do not know how to modify somewhere in the compilation process to copy directly to make it, if someone knows how to do .please tell me ,thank you)

sudo cp -r /home/rnd2/work/maaxboard/zeus/imx-yocto-bsp/maaxboard/build/tmp/sysroots-components/x86_64/python3-pycrypto-native/usr/lib/python3.7/site-packages/Crypto /opt/fsl-imx-wayland-lite/5.4-zeus/sysroots/x86_64-pokysdk-linux/usr/lib/python3.7/site-packages/.

 

 

 

I have found the solution.

please install pycryptodome==3.7 on host opensuse mechine:

pip install pycryptodome==3.7
----
Before I played the old board maaxboard, the python is 2.6, but now it's 3.7. so need to install it.
sometimes ,I am confuse that the pycryptodome should be install in yocto toolcains (DEPENDS += "python3-pycryptodome-native python3-pyelftools-native") or in host machine.

I can find DEPENDS += "python3-pycryptodome-native python3-pyelftools-native" in optee_os.bb file,
so I installed my toolchains in my another ubuntu 18.or host machine. the compilation is passed ! so I thought the error was not in toolchain itself. it should be in host machine.
so I installed : pip install pycryptodome==3.7 on opensuse host. solved it!

0 Kudos
Reply
4,013 Views
gonewithwind-peter
Senior Contributor I

finally, I have found the solutions. I did it 2 years ago for imx7 board. I remember again.
do not need to modify the recipe.
the toolchain does not include the Crypto package
just manually copy Crypto to toolchain(I do not know how to modify somewhere in the compilation process to copy directly to make it, if someone knows how to do .please tell me ,thank you)

sudo cp -r /home/rnd2/work/maaxboard/zeus/imx-yocto-bsp/maaxboard/build/tmp/sysroots-components/x86_64/python3-pycrypto-native/usr/lib/python3.7/site-packages/Crypto /opt/fsl-imx-wayland-lite/5.4-zeus/sysroots/x86_64-pokysdk-linux/usr/lib/python3.7/site-packages/.

0 Kudos
Reply