yocto mono layer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

yocto mono layer

3,522件の閲覧回数
tüskemáté
Contributor I

   Hi,

I'm working on a system where i can run c# applications in raspberry pi. I'm just switched to yocto rocko, and somehow now I always fail on the do_package_qa task. This is my error message:

ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/3.5-api/Microsoft.Build.Engine.dll contained in package mono-libs-3.5 requires mono(System.Xml), but no providers found in RDEPENDS_mono-libs-3.5? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/3.5-api/Microsoft.Build.Utilities.v3.5.dll contained in package mono-libs-3.5 requires mono(System), but no providers found in RDEPENDS_mono-libs-3.5? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/3.5-api/Microsoft.Build.Engine.dll contained in package mono-libs-3.5 requires mono(mscorlib), but no providers found in RDEPENDS_mono-libs-3.5? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(mscorlib), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(System.Xml), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(System), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(System.Configuration), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/mono-configuration-crypto/4.5/Mono.Configuration.Crypto.dll contained in package mono-configuration-crypto requires mono(Mono.Security), but no providers found in RDEPENDS_mono-configuration-crypto? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.6-api/Mono.Debugger.Soft.dll contained in package mono-api-4.6 requires mono(Mono.Cecil), but no providers found in RDEPENDS_mono-api-4.6? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.6.2-api/Mono.Debugger.Soft.dll contained in package mono-api-4.6.2 requires mono(Mono.Cecil), but no providers found in RDEPENDS_mono-api-4.6.2? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.7-api/Mono.Debugger.Soft.dll contained in package mono-api-4.7 requires mono(Mono.Cecil), but no providers found in RDEPENDS_mono-api-4.7? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/xbuild/Microsoft/NuGet/Microsoft.NuGet.Build.Tasks.dll contained in package mono-xbuild requires mono(mscorlib), but no providers found in RDEPENDS_mono-xbuild? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.6.1-api/Mono.Debugger.Soft.dll contained in package mono-api-4.6.1 requires mono(Mono.Cecil), but no providers found in RDEPENDS_mono-api-4.6.1? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/gac/Mono.Messaging.RabbitMQ/4.0.0.0__0738eb9f132ed756/Mono.Messaging.RabbitMQ.dll contained in package mono-gac requires mono(mscorlib), but no providers found in RDEPENDS_mono-gac? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA Issue: /usr/lib/mono/4.5/Microsoft.CodeAnalysis.Scripting.dll contained in package mono-libs-4.5 requires mono(System.Runtime.Loader), but no providers found in RDEPENDS_mono-libs-4.5? [file-rdeps] 
ERROR: mono-5.4.1.6-r0 do_package_qa: QA run found fatal errors. Please consider fixing them. 
ERROR: mono-5.4.1.6-r0 do_package_qa: Function failed: do_package_qa

My mono version is 5.8.0.108 from http://download.mono-project.com/repo/ubuntu  and I'm using xenial ubuntu. The local.conf is now the sample from here:https://git.yoctoproject.org/cgit.cgi/poky/plain/meta-poky/conf/local.conf.sample . 

Any suggestion?

regards

Matthew

ラベル(1)
タグ(3)
2 返答(返信)

2,868件の閲覧回数
a_spin
Contributor I

I'm experiencing the same problem.

Did this document solve you're problem, I didn't find a clue in it.

Regards,

Alberto

0 件の賞賛
返信

2,868件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Matthew,

The Mono layer is not present on the i.MX BSPs so I’m not familiar with it, but there seems to be problems with dependencies for adding mono. If you are using Yocto perhaps the following document on the Yocto Project Wiki may help.

https://wiki.yoctoproject.org/wiki/Building_and_running_embedded_Linux_.NET_applications_from_first_...

Regards,