yocto engineering problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

yocto engineering problem

1,175 Views
logic887
Contributor III

hello

     When I pulled the yocto project from https://github.com/nxp-imx/meta-nxp-desktop/tree/lf-6.1.1-1.0.0-langdale,An issue occurred after compiling with the bitbake imx-image-desktop command:

xueyf_0-1695862253228.png

The host I used was ubuntu18.04,How to solve this problem

0 Kudos
Reply
1 Reply

1,155 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @logic887 

To check the error log, log.do_compile might find details to help fix the do_compile error. 

Have you followed the IMX_YOCTO_PROJECT_USERS_GUIDE_LF6.1.1_1.0.0.pdf for host package? and the recommended minimum Ubuntu version is 20.04 or later. 

You will find Yocto user guide from the link: L6.1.1_1.0.0_LINUX_DOCS (nxp.com)

 

Best regards

Harvey

0 Kudos
Reply