Hello, I use i.MX6qsabresd platform and fsl-yocto-3.14.28 BSP
I use a lvds screen on the imx6qsabresd borad.
I input the following command
(1)MACHINE=imx6qsabresd source fsl-setup-release.sh –b build-fb –e fb
(2)Edit yocto/build/conf/bblayers.conf to add the meta-qt5 layer at the end:
${BSPDIR}/sources/meta-qt5 \
${BSPDIR}/sources/meta-openembedded/meta-ruby \
${BSPDIR}/sources/meta-openembedded/meta-multimedia \
(3)Edit yocto/build/conf/local.conf
EXTRA_IMAGE_FEATURES = "debug-tweaks ssh-server-openssh "
IMAGE_INSTALL_append = " gcc g++ binutils libgcc libgcc-dev libstdc++ libstdc++-dev libstdc++-staticdev \
autoconf automake ccache chkconfig glib-networking glibmm \
packagegroup-core-buildessential pkgconfig \
boost cmake zlib glib-2.0 packagegroup-fsl-tools-testapps \
ruby \
cpufrequtils \
nano \
gdb \
gstreamer \
gst-meta-video \
gst-fsl-plugin \
gst-plugins-base-app \
gst-plugins-base \
gst-plugins-good \
gst-plugins-good-rtsp \
gst-plugins-good-udp \
gst-plugins-good-rtpmanager \
gst-plugins-good-rtp \
gst-plugins-good-video4linux2 \
openssh-sftp-server \
packagegroup-fsl-gstreamer \
packagegroup-fsl-tools-testapps \
packagegroup-fsl-tools-benchmark \
imx-vpu \
imx-test \
qtbase-fonts \
qtbase-plugins \
qtbase-tools \
qtbase-examples \
qtdeclarative \
qtdeclarative-plugins \
qtdeclarative-tools \
qtdeclarative-examples \
qtdeclarative-qmlplugins \
qtmultimedia \
qtmultimedia-plugins \
qtmultimedia-examples \
qtmultimedia-qmlplugins \
qtsvg \
qtsvg-plugins \
qtsensors \
qtimageformats-plugins \
qtsystems \
qtsystems-tools \
qtsystems-examples \
qtsystems-qmlplugins \
qtscript \
qt3d \
qt3d-examples \
qt3d-qmlplugins \
qt3d-tools \
qtwebkit \
qtwebkit-examples-examples \
qtwebkit-qmlplugins \
qtgraphicaleffects-qmlplugins \
qtconnectivity-qmlplugins \
qtlocation-plugins \
qtlocation-qmlplugins \
cinematicexperience \
cairo pango fontconfig freetype pulseaudio dbus \
alsa-lib alsa-tools alsa-state alsa-utils-alsaconf fsl-alsa-plugins \
i2c-tools \
"
DISTRO_FEATURES_remove = "x11 wayland"
(4bitbake fsl-image-qt5
builds was successfull,I flash the rootfs.tar.gz on the arm board,can display Yocto Project,
but can't display any on the screen,like this command: cat wall-1024x768-565.rgb > /dev/fb0
I found My QT5 only support as below:
Available platform plugins are: minimal, offscreen, wayland, wayland-xcomposite-egl, xcb
Also can not display qt5 examples
help me ,thanks.