yocto compile

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

yocto compile

1,901 Views
kaikaisi
Contributor I

WARNING: The license listed MIT was not in the licenses collected for packagegroup-core-x11-xserver

| WARNING: The license listed MIT was not in the licenses collected for packagegroup-base

| WARNING: The license listed MIT was not in the licenses collected for packagegroup-fsl-gstreamer1.0

| WARNING: The license listed MIT was not in the licenses collected for packagegroup-base

| ls: cannot access /home/lja/fsl-release-bsp/build_x11/tmp/sysroots/imx6qsabresd/pkgdata/runtime-reverse/wpa-supplicant-wl18xx: No such file or directory

| readlink: missing operand

| Try `readlink --help' for more information.

| basename: missing operand

| Try `basename --help' for more information.

| WARNING: exit code 1 from a shell command.

| DEBUG: Python function do_rootfs finished

| ERROR: Function failed: license_create_manifest (log file is located at /home/lja/fsl-release-bsp/build_x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-gui/1.0-r0/temp/log.do_rootfs.3120)

ERROR: Task 7 (/home/lja/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-demos/recipes-fsl/images/fsl-image-gui.bb, do_rootfs) failed with exit code '1'

NOTE: Tasks Summary: Attempted 6233 tasks of which 6232 didn't need to be rerun and 1 failed.

No currently running tasks (6232 of 6234)

Summary: 1 task failed:

   /home/lja/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-demos/recipes-fsl/images/fsl-image-gui.bb, do_rootfs

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

Labels (2)
0 Kudos
Reply
2 Replies

1,156 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello kaikai si,

Following up on Biyong Sun, I would recommend reviewing the documentation of the BSP that you are using, which may either be the Freescale Community BSP or the Freescale BSP Release.

You should have no problem baking the fsl-image-gui image as long as the environment is correctly set for your Machine(Board) and that the EULA has been accepted.

0 Kudos
Reply

1,156 Views
BiyongSUN
NXP Employee
NXP Employee

Freescale BSP has been released to customer thounds. And all BSP released has been QA.

And the build system is yocto, if have build issue with standard BSP release. Please check you build environment refer to the Yocto official site.

0 Kudos
Reply