yocto bitbake fsl-image-gui fail(python)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

yocto bitbake fsl-image-gui fail(python)

6,500件の閲覧回数
echozeng
Contributor III

Dear All,

      when I bitbake fsl-image-gui ,show fail log:

      

Loading cache: 100% |###############################################################################################| ETA: 00:00:00
Loaded 2565 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)
NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg

Build Configuration:
BB_VERSION = "1.26.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6ulevk"
DISTRO = "poky"
DISTRO_VERSION = "1.8"
TUNE_FEATURES = "arm armv7a vfp neon callconvention-hard cortexa7"
TARGET_FPU = "vfp-neon"
meta
meta-yocto = "(nobranch):83aa565d93aacae484976562ef1ae8dbbb6b2bc0"
meta-oe
meta-multimedia = "(nobranch):10d3c8f85280a0bf867a8e4f84bcda81c290d28e"
meta-fsl-arm = "(nobranch):c5326c90d6754c8630504ae29244907b0841c3a9"
meta-fsl-arm-extra = "(nobranch):436b86e3421736216412bdbb21cd9cb08c758c75"
meta-fsl-demos = "(nobranch):836bdf5a9d500ed258f1ddc07d89eca74a704098"
meta-bsp
meta-sdk = "(nobranch):2f59ef1080f616f391b1c488fb2204e570f90239"
meta-browser = "(nobranch):4b27058a8275a5310161459c9bb8f4c52a77762c"
meta-gnome
meta-networking
meta-python
meta-ruby
meta-filesystems = "(nobranch):10d3c8f85280a0bf867a8e4f84bcda81c290d28e"
meta-qt5 = "(nobranch):fc026381545650e10fdd488d5b2a3b2d78f87793"

NOTE: Preparing RunQueue
WARNING: /home/build/work/fsl-arm-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_3.14.38.bb.do_compile is tainted from a forced run
WARNING: /home/build/work/fsl-arm-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2015.04.bb.do_compile is tainted from a forced run
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: Function failed: do_install (log file is located at /home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/work/x86_64-linux/python-distribute-native/0.6.32-ml5/temp/log.do_install.19405)
ERROR: Logfile of failure stored in: /home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/work/x86_64-linux/python-distribute-native/0.6.32-ml5/temp/log.do_install.19405
Log data follows:
| DEBUG: Executing shell function do_install
| Before install bootstrap.
| Scanning installed packages
| No setuptools distribution found
| running install
| running bdist_egg
| running egg_info
| writing distribute.egg-info/PKG-INFO
| writing top-level names to distribute.egg-info/top_level.txt
| writing dependency_links to distribute.egg-info/dependency_links.txt
| writing entry points to distribute.egg-info/entry_points.txt
| reading manifest file 'distribute.egg-info/SOURCES.txt'
| reading manifest template 'MANIFEST.in'
| writing manifest file 'distribute.egg-info/SOURCES.txt'
| installing library code to build/bdist.linux-x86_64/egg
| running install_lib
| running build_py
| copying distribute.egg-info/PKG-INFO -> build/bdist.linux-x86_64/egg/EGG-INFO
| copying distribute.egg-info/SOURCES.txt -> build/bdist.linux-x86_64/egg/EGG-INFO
| copying distribute.egg-info/dependency_links.txt -> build/bdist.linux-x86_64/egg/EGG-INFO
| copying distribute.egg-info/entry_points.txt -> build/bdist.linux-x86_64/egg/EGG-INFO
| copying distribute.egg-info/top_level.txt -> build/bdist.linux-x86_64/egg/EGG-INFO
| creating 'dist/distribute-0.6.32-py2.7.egg' and adding 'build/bdist.linux-x86_64/egg' to it
| Traceback (most recent call last):
| File "setup.py", line 250, in <module>
| scripts = scripts,
| File "/home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/x86_64-linux/usr/lib/python2.7/distutils/core.py", line 151, in setup
| dist.run_commands()
| File "/home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/x86_64-linux/usr/lib/python2.7/distutils/dist.py", line 953, in run_commands
| self.run_command(cmd)
| File "/home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/x86_64-linux/usr/lib/python2.7/distutils/dist.py", line 972, in run_command
| cmd_obj.run()
| File "/home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/work/x86_64-linux/python-distribute-native/0.6.32-ml5/distribute-0.6.32/setuptools/command/install.py", line 73, in run
| self.do_egg_install()
| File "/home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/work/x86_64-linux/python-distribute-native/0.6.32-ml5/distribute-0.6.32/setuptools/command/install.py", line 93, in do_egg_install
| self.run_command('bdist_egg')
| File "/home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/x86_64-linux/usr/lib/python2.7/distutils/cmd.py", line 326, in run_command
| self.distribution.run_command(command)
| File "/home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/x86_64-linux/usr/lib/python2.7/distutils/dist.py", line 972, in run_command
| cmd_obj.run()
| File "/home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/work/x86_64-linux/python-distribute-native/0.6.32-ml5/distribute-0.6.32/setuptools/command/bdist_egg.py", line 241, in run
| dry_run=self.dry_run, mode=self.gen_header())
| File "/home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/work/x86_64-linux/python-distribute-native/0.6.32-ml5/distribute-0.6.32/setuptools/command/bdist_egg.py", line 542, in make_zipfile
| visit(z, dirname, files)
| File "/home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/work/x86_64-linux/python-distribute-native/0.6.32-ml5/distribute-0.6.32/setuptools/command/bdist_egg.py", line 532, in visit
| z.write(path, p)
| File "/home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/x86_64-linux/usr/lib/python2.7/zipfile.py", line 1125, in write
| mtime = time.localtime(st.st_mtime)
| SystemError: new style getargs format but argument is not a tuple
| ERROR: python setup.py install execution failed.
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_install (log file is located at /home/build/work/fsl-arm-yocto-bsp/build-fb/tmp/work/x86_64-linux/python-distribute-native/0.6.32-ml5/temp/log.do_install.19405)
ERROR: Task 954 (virtual:native:/home/build/work/fsl-arm-yocto-bsp/sources/poky/meta/recipes-devtools/python/python-distribute_0.6.32.bb, do_install) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2128 tasks of which 2127 didn't need to be rerun and 1 failed.
No currently running tasks (2127 of 4181)

Summary: 1 task failed:
virtual:native:/home/build/work/fsl-arm-yocto-bsp/sources/poky/meta/recipes-devtools/python/python-distribute_0.6.32.bb, do_install
Summary: There were 2 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.

How to fixed it?  host os is ubuntu 14.04(64bit) lts.

Thanks.

0 件の賞賛
返信
11 返答(返信)

5,180件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi,

From [1][2] seems to be a python version problem. On my system, I have python 2.7.6 and the problem is not reproducible. What's your python version? (python --version) .

Thank you,

Marius

[1] python 2.7 - SystemError: new style getargs format but argument is not a tuple - Stack Overflow 

[2] [Python-Dev] SystemError: new style getargs format but argument is not a tuple 

0 件の賞賛
返信

5,180件の閲覧回数
echozeng
Contributor III

python version is 2.7.6 on my system.

0 件の賞賛
返信

5,180件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Perhaps it makes sense to create (separate) Virtual Machine with Ubuntu 14.04 and try all again.   

Regards,

Yuri.

0 件の賞賛
返信

5,180件の閲覧回数
echozeng
Contributor III

What is 'try all '?

Your meaning is delete dir build-fb and start from "MACHINE=imx6ulevk source fsl-setup-release.sh -b build-fb -e fb"  ?

0 件の賞賛
返信

5,180件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  I meant install new Ubuntu and new Yocto.    

Regards,

Yuri.

0 件の賞賛
返信

5,180件の閲覧回数
echozeng
Contributor III

How to install new Yocto?

Don't tell me refer to  'i.MX_Yocto_Project_User's_Guide.pdf' again!

My Ubuntu is  new installation ,Then I refer to 'i.MX_Yocto_Project_User's_Guide.pdf' to get Yocto Project. Now I want to know who can tell me  the exact answer to fixed what I met!

0 件の賞賛
返信

5,180件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  From Yocto Project Reference Manual :

1.3.3. Required Git, tar, and Python Versions

In order to use the build system, your host development system must meet the following version requirements for Git, tar, and Python:

  • Git 1.8.3.1 or greater

  • tar 1.24 or greater

  • Python 3.4.0 or greater

Regards,

Yuri.

0 件の賞賛
返信

5,180件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Please check if host environment is setup correctly.
Please use section 3 (Host Setup) of "i.MX_Yocto_Project_User's_Guide.pdf".

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... 

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,180件の閲覧回数
echozeng
Contributor III

I check the section 3 of "i.MX_Yocto_Project_User's_Guide.pdf", No problem be found. The packages is already the newest version.

0 件の賞賛
返信

5,180件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Can you try to build core-image-minimal version first (from scratch) ?   

Regards,

Yuri.

0 件の賞賛
返信

5,180件の閲覧回数
echozeng
Contributor III

it's OK, just building fsl-image-gui fail.

0 件の賞賛
返信