yocot sdk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

yocot sdk

1,507件の閲覧回数
玉栋郭
Contributor III

hi all

i  use the The following command build sdk.

bitbake fsl-image-qt5 -c populate_sdk

I‘m trying build linux kernel with yocot sdk,  but which linux  config is the imx6Q sabreSD config?  

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,393件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   For recent BSPs :

$ DISTRO=fsl-imx-fb MACHINE=imx6qsabresd source fsl-setup-release.sh –b build-fb

$ bitbake fsl-image-qt5 -c populate_sdk

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

0 件の賞賛
返信