xorg.conf for iMX53 with TSLIB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

xorg.conf for iMX53 with TSLIB

1,693 次查看
dirtyfishtank
Contributor I

Hey all,

I'm having some problems getting xorg to behave correctly on a iMX53 touchscreen. When my device first starts X, it switches mouse protocols a few times until it gets to ps/2 (see below), then when I touch the screen the X menu appears momentarily but the cursor never moves. I'm using TSLIB, and I am able to run ts_calibrate and ts_test with no problem, but that's the only application that allows me to move the cursor and click on the screen. This makes me think it is a problem with the config file xorg.conf. Does anyone have any ideas or suggestions as to what I should try or any hints on the xorg config file below? thanks?

Output after starting X:

_XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6

_XSERVTransOpen: transport open failed for inet6/iND16599:0

_XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6

(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base

(EE) XKB: No components provided for device Virtual core keyboard

(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base

(EE) XKB: No components provided for device (unnamed keyboard)

Switching to mouse protocol "imps/2"

Switching to mouse protocol "exps/2"

Switching to mouse protocol "bus"

Switching to mouse protocol "ps/2"

Xorg.conf

Section "InputDevice"

        Identifier      "Generic Keyboard"

        Driver          "kbd"

        Option          "XkbRules"      "xorg"

        Option          "XkbModel"      "pc105"

        Option          "XkbLayout"     "us"

EndSection

Section "InputDevice"

        Identifier      "Configured Mouse"

        Driver          "mouse"

        Option          "CorePointer"

        Option          "Protocol" "ps/2" #has no effect

        Option          "Device" "/dev/input/event2" #has no effect

EndSection

Section "Device"

        Identifier      "i.MX Accelerated Framebuffer Device"

        Driver          "imx"

        Option          "fbdev"         "/dev/fb0"

# This option only recognized when "mxc_epdc_fb" frame buffer driver in

# use.  Values are "RGB565" (default, 16-bit RGB), "Y8" (8-bit gray),

# and "Y8INV" (8-bit gray inverted).

        Option          "FormatEPDC"    "Y8INV"

EndSection

Section "Monitor"

        Identifier      "Configured Monitor"

EndSection

Section "Screen"

        Identifier      "Default Screen"

        Monitor         "Configured Monitor"

        Device          "i.MX Accelerated Framebuffer Device"

EndSection

Section "ServerLayout"

        Identifier      "Default Layout"

        Screen          "Default Screen"

EndSection

标签 (3)
标记 (3)
0 项奖励
回复
0 回复数