xinput_calibrator error when xserver using GPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

xinput_calibrator error when xserver using GPU

3,305件の閲覧回数
westbrook
Contributor III

Hello guys,

I am using X11 and vivante GPU driver. Environment is as following:

HW: imx6 solo

SW: kernel-4.9.11,  GPU driver 6.2.2.p0, GPU packages of filesystem:

imx-gpu-viv-6.2.2

gpu-viv-g2d-6.2.2

xf86-video-imx-viv-6.2.2.p0

Now I can start X server successfully with GPU driver.

1. Then I run a X client -- xinput_calibrator to check whether X work fine. Test steps:

X &

xinput_calibrator --output-type xinput -v

Got following errors:

free(): invalid pointer
terminate called after throwing an instance of 'std::runtime_error'
  what():  Unable to connect to X server

The detailed log is attached x11_gpu_1015_1.log

Then Xserver is stopped. I checked the source code of xinput_calibrator, it seems that XOpenDisplay() returns NULL, Then the "std::runtime_error"  " Unable to connect to X server" is shown.

Why does this happen?

2. I configure the xserver to use framebuffer, not use vivante driver:

/etc/X11/xorg.conf

Then I start Xserver with framebuffer, and execute xinput_calibrator, it works fine, and display well. See x11_fb_1015_1.log

Can anyone help me check this issue?

Thank you so much.

Best Regards,

Xiao

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,924件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Did you set this?

$ export DISPLAY=:0.0
0 件の賞賛
返信

2,924件の閲覧回数
westbrook
Contributor III

Hi Jimmy,

Thanks for your reply. I checked the environment variables, DISPLAY=:0. Is this value OK?

I have tried following version, the xinput_calibrator can work with Xserver:

SW: kernel-4.9.11,  GPU driver 6.2.2.p0, GPU packages of filesystem:

imx-gpu-viv-5.0.11.p8.6

xf86-video-imx-viv-5.0.11.p8.6

Is there any version limitations? like 5.0.11.p8.6 library packages must use kernel GPU driver 5.0.11.p8.6 ?

BR,

Xiao

0 件の賞賛
返信