wm8962 no operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

wm8962 no operation

1,862件の閲覧回数
kimsangyoung
Contributor I

I'm made new board using i.mx6q cpu . The media player was operated using a video . However , the audio is off.

Check the results wm8962 audio ic signal MCLK is ok, LRCLK and Bit clk is not displayed.

Does anyone know why this signal no output ? The device is connected to I2C1.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,729件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi kim

suggest to check hardware with SDK (wm8962.c test)

i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6 series, including

reusable drivers and tests for many peripherals, and much example code.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,729件の閲覧回数
kimsangyoung
Contributor I

Dear igor

thank you for your kindly answer.

I will test use by i.MX 6Series Platform SDK

Best regards

sykim

0 件の賞賛
返信