win 7 doesnt recognize imx6sl custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

win 7 doesnt recognize imx6sl custom board

1,347件の閲覧回数
shlomiperlman
Contributor II

Hi,

i connected the production board to the PC (win 7) and the device manager displays it as "Unknown device"

if its not recognized as HID device i cannot use the MFG tool.

is it a driver issue or something else?

where can i find the imx6sl windows drivers?

thanks,

ラベル(1)
0 件の賞賛
返信
1 返信

1,256件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi shlomi

please check boot pins, 24MHz clock and try suggestions on

Mfgtool can't connect in windows7

use latest mfg tools, no need for special driver

IMX6_L4.1.15_1.2.0_MFG_TOOL

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信