win 7 doesnt recognize imx6sl custom board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

win 7 doesnt recognize imx6sl custom board

920 次查看
shlomiperlman
Contributor II

Hi,

i connected the production board to the PC (win 7) and the device manager displays it as "Unknown device"

if its not recognized as HID device i cannot use the MFG tool.

is it a driver issue or something else?

where can i find the imx6sl windows drivers?

thanks,

标签 (1)
0 项奖励
回复
1 回复

829 次查看
igorpadykov
NXP Employee
NXP Employee

Hi shlomi

please check boot pins, 24MHz clock and try suggestions on

Mfgtool can't connect in windows7

use latest mfg tools, no need for special driver

IMX6_L4.1.15_1.2.0_MFG_TOOL

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复