wifi module is not working (rtl8192eu).

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

wifi module is not working (rtl8192eu).

1,867 次查看
diwakar2599
Contributor II

Once i connected my Wi-Fi module (rtl8192eu) my module is detected but while using ifconfig my module is not showing so I checked wireless communication on imx in that while using  wpa_cli  for selecting the network I am facing this type of error

 

 

Copyright (c) 2004-2022, Jouni Malinen <j@wl.fi> and contributors

This software may be distributed under the terms of the BSD license. See README for more details.

DO

Interactive mode

Could not connect to wpa_supplicant: (nil) re-trying

 

 

pls help me to solve this issue

0 项奖励
回复
3 回复数

1,854 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Your Wi-Fi module is a USB Wi-Fi dongle, isn't it?

Best regards.

Jorge

0 项奖励
回复

1,838 次查看
diwakar2599
Contributor II
It is Realtek usb WIFI module rtl8192eu.
@JorgeCas.
0 项奖励
回复

1,825 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Researching about this function with internal team, our BSP does not support USB Wi-Fi, you can consult it on release notes.

Jorge7u7_0-1684880807987.png

Best regards.

Jorge.