wifi model selection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

wifi model selection

3,615 次查看
gaobo
Contributor I

Hi :

bsp:4.14.78

machine:imx8m

In imx8mq-evk platform,we test wifi use qca6174 model.But now we want to make product,but due to module import problem,we need each other to replace.how about adm8211 or what would you think about?

thinks!

0 项奖励
回复
5 回复数

3,498 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Dear Gao bo,

>>how about adm8211 or what would you think about?

I checked ADM8211  datasheet, the WIFI module uses PCI interface, which is not supported by i.MX8MQ. So you can't select it.

pastedImage_7.png

pastedImage_8.png

>>Inferface of I.MX8MQ for WIFI module

---SDIO interface

---PCIe interface

---USB interface

The WIFI module you select must support one of above interface. Actually you have many choice , such as NXP's wifi , Broadcomm, QCA, Realtek etc.

1. NXP's WIFI

Wi-Fi&reg + Bluetooth | NXP 

pastedImage_4.png

2. Others

----QCA9880 with PCIe interface

----INTEL9260 with PCIe interface

Some customers have successfully used them.

----LBEE5KL1PJ based on QCA9377 with SDIO interface

the module is supported by i.MX8M Mini.

>>Software

you don't need to worry about software, even if our linux BSP doen't support the WIFI module you select by default, you can also port it to our linux BSP. Generally speaking, you should ask provider to give you materials below:

(1) Poring documents for you linux bsp version.

(2) Drivers for SDIO or PCIe interface.

(3) Firmware.

Hope above contents are helpful to you!

Have a nice day!

B.R,

Weidong

0 项奖励
回复

3,498 次查看
gaobo
Contributor I

Hi wigros Sun:

Actually,we want to find wifi+ble model(wifi模组),not wifi chip ,because we dont want to do RF section.

Do you have any recommendations?

thanks!

0 项奖励
回复

3,498 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Gao bo,

   I will send some information to you by personal email.

check it, please!

Have a nice day!

B.R,

weidong

0 项奖励
回复

3,498 次查看
gaobo
Contributor I

Hi Wigros Sun:

I get it , thank you very much Wigros Sun!

Send you good wishes.

0 项奖励
回复

3,498 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Got it,

You are welcome!

weidong

0 项奖励
回复