wifi error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

wifi error

Jump to solution
4,637 Views
stevenwoo
Contributor I

Dear all:

In i.MX50 evk Android 10.3 , I try to enable the wifi function but  the "wifi error" message show up. How can make that works? 

Best regard

Steven Wu

Labels (1)
0 Kudos
Reply
1 Solution
4,431 Views
PeterChan
NXP Employee
NXP Employee

No, MX50 EVK board does not possess any wifi and bluetooth modules. The most handy way to test wifi is to look for a SDIO wifi card with atheros chip inside.

View solution in original post

0 Kudos
Reply
7 Replies
4,431 Views
PeterChan
NXP Employee
NXP Employee

Hello Steven,

Can you attach the error log here?

If you are using the clean r10.3 release on i.MX50 RD3 EVK board, please make sure you have applied this patch. It enables the 3.15V power to supply the wifi module.

Regards,

Peter

0 Kudos
Reply
4,431 Views
stevenwoo
Contributor I

Dear Peter

Thanks for this wifi patch file!

Which directory should I need to put?

0 Kudos
Reply
4,431 Views
PeterChan
NXP Employee
NXP Employee

Hello Steven,

The patch is for kernel. Please update this file to /kernel_imx/arch/arm/mach-mx5/mx50_rdp.c.


0 Kudos
Reply
4,431 Views
stevenwoo
Contributor I

The platform i.MX50 EVK what I used is 700-26721 REV B , SCH-26721 REV D1.IMG_5899.JPG I try but it still show "wifi error"!

0 Kudos
Reply
4,431 Views
PeterChan
NXP Employee
NXP Employee

Do you have any wifi module connecting to the EVK board? If yes, please follow the user guide to enable  wifi.

0 Kudos
Reply
4,431 Views
stevenwoo
Contributor I

Does that EVK board has built-in wifi and bluetooth?

0 Kudos
Reply
4,432 Views
PeterChan
NXP Employee
NXP Employee

No, MX50 EVK board does not possess any wifi and bluetooth modules. The most handy way to test wifi is to look for a SDIO wifi card with atheros chip inside.

0 Kudos
Reply