why is touchscreen calibration taking forever?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why is touchscreen calibration taking forever?

1,870 Views
danix
Contributor III

In my custom board I have a four wire resistive TS connected to the imx LRADC as in the EVK...

when I ran ts_calibrate it takes like 15 minuites to change the test points

does the ts caliberation has something to do with the panel selected, b/c it's fast when I'm using the default panel driver (LMS430),...all the problem show up after I edited the driver to my specific panel (320x240 3.5"....

Regards

Tags (1)
0 Kudos
Reply
2 Replies

1,707 Views
danix
Contributor III

Hi Eduardo,

 

This is an old thread, I have solved the problem minuets after I posted it here though, It was a hardware problem

0 Kudos
Reply

1,707 Views
G_rio
Contributor III
I'm using imx53 and i had had the same problem. It was fixed with an update manufactory drive.
0 Kudos
Reply