why is touchscreen calibration taking forever?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

why is touchscreen calibration taking forever?

1,312 次查看
danix
Contributor III

In my custom board I have a four wire resistive TS connected to the imx LRADC as in the EVK...

when I ran ts_calibrate it takes like 15 minuites to change the test points

does the ts caliberation has something to do with the panel selected, b/c it's fast when I'm using the default panel driver (LMS430),...all the problem show up after I edited the driver to my specific panel (320x240 3.5"....

Regards

标记 (1)
0 项奖励
回复
2 回复数

1,149 次查看
danix
Contributor III

Hi Eduardo,

 

This is an old thread, I have solved the problem minuets after I posted it here though, It was a hardware problem

0 项奖励
回复

1,149 次查看
G_rio
Contributor III
I'm using imx53 and i had had the same problem. It was fixed with an update manufactory drive.
0 项奖励
回复