who have the patch about pcie bus on the linux 3.0.35?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

who have the patch about pcie bus on the linux 3.0.35?

706 次查看
xiuqingchang
Contributor I

who have the patch about pcie bus on the linux 3.0.35?

I work on the imx6q ,when i debug pcie bus on the linux 3.0.35,there is some problem,however on the linux3.10.17,it's ok,so i want to have the patch about pcie on the linux3.0.35,or tell me the difference between linux 3.0.35 and linux3.10.17 about pcie bus;thanks

0 项奖励
回复
1 回复

607 次查看
art
NXP Employee
NXP Employee

There is no separate patch for that since some problems of the 3.0.35 BSP (not only related with PCIe) were on the kernel level and newer kernel should be used to fix them.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复