What are the Voice Recognition options available in iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What are the Voice Recognition options available in iMX6

1,040件の閲覧回数
keshavakumarb
Contributor I

Hello,

I want to know the voice detection/recognition support in imx6 via external microphone. How can I achieve this??

Thank you in advance.

ラベル(6)
タグ(3)
0 件の賞賛
返信
1 返信

871件の閲覧回数
art
NXP Employee
NXP Employee

There are no any voice recognition acceleration capabilities on the hardware level in the i.MX6 series processors. All this is software dependent. For example, if you run Android, you can use its voice recognition/control capabilities etc.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信