while building the Android platform for i.MX8 processor with imx- automotive-13.0.0_1.3.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

while building the Android platform for i.MX8 processor with imx- automotive-13.0.0_1.3.0

851件の閲覧回数
shrinithi
Contributor I

In generating the i.MX8 Android release source code build environment. I followed this commands only

$ mkdir ~/bin
$ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$ chmod a+x ~/bin/repo
$ export PATH=${PATH}:~/bin
$ source ~/imx-automotive-13.0.0_1.3.0/imx_android_setup.sh

in source the imx_android_setup.sh file it shows like

Start fetching the source for android build
Setting REL_PACKAGE_DIR to /home/imx-automotive-13.0.0_1.3.0
Setting WORKSPACE to /home
Setting android_builddir to /home/android_build
Downloading Repo source from https://gerrit.googlesource.com/git-repo

... A new version of repo (2.35) is available.
... You should upgrade soon:
cp /home/hsx1cob/android_build/.repo/repo/repo /home/bin/repo


Your identity is: <><>name and email are shown correctly
If you want to change this, please re-run 'repo init' with --config-name

repo has been initialized in /home/android_build

... A new version of repo (2.35) is available.
... You should upgrade soon:
cp /home/android_build/.repo/repo/repo /home/bin/repo

remote: Enumerating objects: 1485, done.
remote: Counting objects: 100% (673/673), done.
remote: Compressing objects: 100% (49/49), done.
remote: Total 1485 (delta 647), reused 635 (delta 624), pack-reused 812
Receiving objects: 100% (1485/1485), 371.35 KiB | 65.00 KiB/s, done.
Resolving deltas: 100% (1022/1022), completed with 67 local objects.
Fetching: 0% (0/1153) 0:05 | 4 jobs | 0:04 platform/art @ artReceiving objects:Receiving objects: 100% (879/879), 273.57 KiB | 21.04 MiB/s, done.
Resolving deltas: 100% (16/16), done.
Fetching: 0% (0/1153) 1:26 | 4 jobs | 1:26 platform/art @ artReceiving objects:Fetching: 0% (0/1153) 1:27 | 4 jobs | 1:27 platform/art @ artReceiving objects:Receiving objects: 100% (16151/16151), 20.02 MiB | 31.73 MiB/s, done.
Resolving deltas: 100% (7459/7459), done.
Fetching: 0% (0/1153) 1:34 | 4 jobs | 1:34 platform/art @ artReceiving objects:Receiving objects: 100% (1065/1065), 363.42 KiB | 24.23 MiB/s, done.
Resolving deltas: 100% (37/37), done.
Fetching: 0% (0/1153) 1:42 | 4 jobs | 1:42 platform/art @ artReceiving objects:Receiving objects: 100% (8308/8308), 4.74 MiB | 34.42 MiB/s, done.
Resolving deltas: 100% (2331/2331), done.
Fetching: 0% (4/1153) 3:38 | 4 jobs | 3:38 platform/art @ artReceiving objects:Fetching: 0% (4/1153) 3:39 | 4 jobs | 3:38 platform/art @ artReceiving objects:Fetching: 0% (4/1153) 3:39 | 4 jobs | 3:39 platform/art @ artReceiving objects:Fetching: 0% (4/1153) 3:40 | 4 jobs | 3:40 platform/art @ artReceiving objects:Fetching: 0% (4/1153) 3:41 | 4 jobs | 3:40 platform/art @ artReceiving objects:Fetching: 0% (4/1153) 3:41 | 4 jobs | 3:41 platform/art @ artReceiving objects:Receiving objects: 100% (182593/182593), 116.36 MiB | 32.57 MiB/s, done.
Fetching: 0% (4/1153) 3:42 | 4 jobs | 3:41 platform/art @ artResolving deltas: Fetching: 0% (4/1153) 3:42 | 4 jobs | 3:42 platform/art @ artResolving deltas: Fetching: 0% (4/1153) 3:43 | 4 jobs | 3:42 platform/art @ artResolving deltas: Fetching: 0% (4/1153) 3:43 | 4 jobs | 3:43 platform/art @ artResolving deltas: Resolving deltas: 100% (84668/84668), done.
Fetching: 0% (4/1153) 4:09 | 4 jobs | 4:09 platform/art @ artReceiving objects:Fetching: 0% (4/1153) 4:10 | 4 jobs | 4:10 platform/art @ artReceiving objects:Fetching: 0% (4/1153) 4:11 | 4 jobs | 4:10 platform/art @ artReceiving objects:Fetching: 0% (4/1153) 4:11 | 4 jobs | 4:11 platform/art @ artReceiving objects:Receiving objects: 100% (41800/41800), 159.44 MiB | 79.80 MiB/s, done.
Resolving deltas: 100% (24081/24081), done.
Fetching: 0% (4/1153) 4:18 | 4 jobs | 4:18 platform/art @ artReceiving objects:Receiving objects: 100% (1942/1942), 1.24 MiB | 48.80 MiB/s, done.
Resolving deltas: 100% (101/101), done.

....

100% (4901/4901), done.
Receiving objects: 100% (8508/8508), 12.61 MiB | 74.23 MiB/s, done.ceiving objects: 0% (1/8508)
Resolving deltas: 100% (3226/3226), done.14:42 platform/cts @ ctsResolving deltas: 100% (3226/3226)
Receiving objects: 100% (1225/1225), 315.43 KiB | 12.62 MiB/s, done.eiving objects: 0% (1/1225)
Resolving deltas: 100% (171/171), done.
Receiving objects: 100% (17444/17444), 12.39 MiB | 45.96 MiB/s, done.iving objects: 95% (16572/17444)
Resolving deltas: 100% (6035/6035), done.
Receiving objects: 100% (12675/12675), 252.78 MiB | 99.71 MiB/s, done.ving objects: 96% (12213/12675), 185.90 MiB | 92.95 MiB/s
Resolving deltas: 100% (4867/4867), done.17:03 platform/cts @ ctsResolving deltas: 71% (3482/4867)
Receiving objects: 100% (10960/10960), 2.35 MiB | 34.89 MiB/s, done.eiving objects: 0% (1/10960)
Resolving deltas: 100% (4166/4166), done.
Receiving objects: 100% (6270/6270), 1.85 MiB | 25.58 MiB/s, done.eceiving objects: 0% (1/6270)
Resolving deltas: 100% (1960/1960), done.
Receiving objects: 100% (1487/1487), 430.83 KiB | 30.77 MiB/s, done.eiving objects: 0% (1/1487)
Resolving deltas: 100% (68/68), done.
Receiving objects: 100% (2838/2838), 730.87 KiB | 29.23 MiB/s, done.eiving objects: 0% (1/2838)
Resolving deltas: 100% (656/656), done.
Receiving objects: 100% (13163/13163), 2.89 MiB | 30.17 MiB/s, done.eiving objects: 26% (3423/13163)
Resolving deltas: 100% (5304/5304), done.
Receiving objects: 100% (1571/1571), 6.75 MiB | 39.04 MiB/s, done.eceiving

 

like this its loading so long hours when it will get complete?, it fetching objects more than 5 hours it seems and Can you please tell me whether is correctly going or not ?and it takes how longs?

thanks and regards

Shrinithi CG

0 件の賞賛
返信
0 返答(返信)