which I.MX6 will allow PAL input and output as well as BT656 input and output?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

which I.MX6 will allow PAL input and output as well as BT656 input and output?

867 次查看
gana
Contributor I

Hi all,

which of the IMX family will allow to take PAL input , BT 656 input , PAL output and BT656 output simultaneously?

what is max configuration possible?

Regards

Rana

标签 (1)
0 项奖励
回复
1 回复

765 次查看
joanxie
NXP TechSupport
NXP TechSupport

i.MX6 can support this, but I don't know what you mean max configuration, which depends what framerate, resoluition, format you use. refer to the Reference Manual, for display,Total raw pixel rate of all interfaces is up to 532 Mpixels/sec, 24 bpp (266 Mpixels/sec per each IPU). for camera, Two Parallel Camera ports (up to 20-bit, up to 240MHz peak each).

for more detailed information, pls refer to the Reference Manual, focus on the Chapter 37 Image Processing Unit (IPU)

0 项奖励
回复