where uboot source code is put in?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

where uboot source code is put in?

1,414 次查看
mingmingyuan
Contributor III

linux 3.0.35  ltlib manger

I can't find uboot source code,can you tell me where uboot source code path?

thanks

标签 (2)
0 项奖励
回复
1 回复

1,306 次查看
igorpadykov
NXP Employee
NXP Employee

Hi mingming

please refer to p.10 attached Linux Guide:

Get the source code of one package.

The source code will be extracted to <ltib folder>/rpm/BUILD/ */

./ltib -m prep -p <package name>

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复