where is u-boot elf file for imx6 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where is u-boot elf file for imx6 processor

1,353 Views
hailiu
Contributor IV

Dear community,

According to this board, the Yocto project has already generated an elf file for u-boot, I already set DEBUG_BUILD = "1" in local.conf, Where is the elf file for u-boot? I want to use it to debug u-boot by using Jlink jtag debugger.

 

thank you,

Hai

0 Kudos
Reply
3 Replies

1,347 Views
hailiu
Contributor IV

found it. It is in u-boot-imx/1_2020.04-r0/git/mx6solosabresd_optee_config

0 Kudos
Reply

1,340 Views
b36401
NXP Employee
NXP Employee

Thanx for letting know. I'm closing the thread.

0 Kudos
Reply

1,351 Views
hailiu
Contributor IV
0 Kudos
Reply