where can i find i.mx family Linux Softwave Development kit Reference Manual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where can i find i.mx family Linux Softwave Development kit Reference Manual

2,147 Views
stevenshan
Contributor II

when i learn the i.mx23 Linux BSP user's guide  which document number is 926-77208 ,it tell me reference: i.mx family Linux Softwave Development kit Reference Manual in page V,where can i download it?

Labels (2)
0 Kudos
Reply
5 Replies

1,904 Views
stevenshan
Contributor II

igor

Thank you very much,it is great!

0 Kudos
Reply

1,904 Views
igorpadykov
NXP Employee
NXP Employee

Hi steven

Linux Manual is included in each BSP package, for i.MX233 EVK :

Supporting Information (5)

i.MX23 EVK Linux Documentation Bundle. (REV 2010.05)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,904 Views
stevenshan
Contributor II

igor

Thanks your reply,but i still confuse .

The file i.MX23 Linux BSP User’s Guide ,Document Number: 926-77208,it tell me For more information about installing the BSP and toolchain for the board, building zImage and root file system, see the i.MX Family Linux Software Development Kit Reference Manual.

i.MX23 EVK Linux Documentation Bundle include The file i.MX23 Linux BSP User’s Guide.pdf,mx23_linux.pdf,i.MX23_Linux_BSP_Release_Note.pdf,evk2010_05_imx23_Linux_QuickStart.pdf,evk2010_05_imx23_Linux_HelloWorld_AN.pdf,but i can not find other files tell me nstalling the BSP and toolchain,building zImage and root file system.

I need your help for more detail.

0 Kudos
Reply

1,904 Views
igorpadykov
NXP Employee
NXP Employee

in this package i.MX Family Linux Software Development Kit Reference Manual is named

as mx23_linux.pdf, for building steps please look at i.MX23 Linux BSP User’s Guide.pdf.

Best regards

igor

1,904 Views
stevenshan
Contributor II

schematic.pnghi ,igor

I make a Printed Circuit Board ,and now the result is not good,which i had tested in below,i wish you can help me.

5V in PIN102 ---VDD5V ,VDDIO --3.126V ,VDD ---1.228 ,VDDA--1.788V ,PIN119 PWS  is 2.22V, VDDM is cycle by 0.26V-0.399V,DC-DC 4P2 1.19V.

boot0--boot4 is all 0V , crystal oscillator is 24V tested by oscilloscope .

I think there are some problems with my circuit,can you help me?

0 Kudos
Reply