where can i find i.MX31 PDK 1.5 Linux User’s Guide

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

where can i find i.MX31 PDK 1.5 Linux User’s Guide

1,027 次查看
stevenshan
Contributor II

The belows is from Developing an Application for the i.MX Devices on the Linux Platform ,but i can not search i.MX31 PDK 1.5 Linux User’s Guide ,where can i find it?

If the user requires any help to set up the prerequisites, refer to the Linux BSP documents. For example,for setting up the i.MX31 PDK, refer to the i.MX31 PDK 1.5 Linux User’s Guide (926-77208), which is available in the BSP tarball that resides in the /doc/ directory.

标签 (2)
0 项奖励
回复
2 回复数

888 次查看
stevenshan
Contributor II

I had found the file below,i think is the file  i.MX31 PDK 1.5 Linux User’s Guide

i.MX31 3-Stack Platform Linux SDK

Standard Release Package User’s Guide

Document Number: 926-77208

Rev. 1.2

02/2008

0 项奖励
回复

888 次查看
igorpadykov
NXP Employee
NXP Employee

it is located on i.MX31 PDK product page, below full links:

Supporting Information (4)

i.MX35 PDK Linux Documentation Bundle (REV 2009.12)

http://www.nxp.com/products/power-management/pmics/pmics-for-i.mx-processors/i.mx35-product-developm...

Board Support Packages (2)

Linux 2.6.31 Source Code Files 2009.12 Release support i.MX23, i.MX25, i.MX35, i.MX51. (REV 2009.12)

http://www.nxp.com/products/power-management/pmics/pmics-for-i.mx-processors/i.mx35-product-developm...

~igor

0 项奖励
回复