Hello Team
From the README file, I can not get any information about the -flags parameters, is it used for the following container flags?
Thank you!
Solved! Go to Solution.
 BiyongSUN
		
			BiyongSUN
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		You want to know the boot flag or container flag?
If it is container flag, it is in the reference manual and as you have already shown them.
and it is about the authentication. not for the imx-mkimage "-flag". It is used by the code-signing tool.
If it is boot flag.
Please refer to System Controller Firmware Porting Guide
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi ZHOUNENG
for imx-mkimage flags one can look at imx-mkimage documentation
https://source.codeaurora.org/external/imx/imx-mkimage/tree/README?h=lf-5.10.y_2.0.0
Best regards
igor
Hello igor
Thanks for help, I can get only the following information from the README file of imx-mkimage git repo.
-flags [value] Specifies flags for the new container. The value needs to be a 32bit value in hex.
 BiyongSUN
		
			BiyongSUN
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		You want to know the boot flag or container flag?
If it is container flag, it is in the reference manual and as you have already shown them.
and it is about the authentication. not for the imx-mkimage "-flag". It is used by the code-signing tool.
If it is boot flag.
Please refer to System Controller Firmware Porting Guide
Hello Biyong
I just also found this boot flags configuration, it is what I want to know. Thank you!.