when my application keep on runing about 10 h,cpu stalls

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

when my application keep on runing about 10 h,cpu stalls

ソリューションへジャンプ
2,385件の閲覧回数
chenghaibo
Contributor III

微信图片_20191127160339.png

the kernel version is 4.14.98, the cpu is imx6q , who can help me, thanks a lot

0 件の賞賛
返信
1 解決策
2,298件の閲覧回数
b36401
NXP Employee
NXP Employee

Possibly there is some memory leakage and lack of the memory hangs the process.
Please try to monitor memory use during the running of the system.
I mean you can do something like "cat /proc/meminfo" every hour in background.

Also possibly bad RAM causes the process to hang.
Please perform DDR stress test.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,298件の閲覧回数
chenghaibo
Contributor III

after calibrate the ddr3 and use the params, the board nerver show this error message again

0 件の賞賛
返信
2,299件の閲覧回数
b36401
NXP Employee
NXP Employee

Possibly there is some memory leakage and lack of the memory hangs the process.
Please try to monitor memory use during the running of the system.
I mean you can do something like "cat /proc/meminfo" every hour in background.

Also possibly bad RAM causes the process to hang.
Please perform DDR stress test.

0 件の賞賛
返信
2,298件の閲覧回数
chenghaibo
Contributor III

may be the develop boad is quickly interact with the net

0 件の賞賛
返信
2,298件の閲覧回数
chenghaibo
Contributor III

thank you very much

0 件の賞賛
返信