Hello experts,
I am running bsp L5.4.24 on i.MX8MM EVK.
I config the GPIO5_13 as a normal GPIO input pin.
and use
devm_request_irq(gpio_dev->dev, gpio_dev->irq, cosmo_gpio_uart_recv_irq,IRQF_TRIGGER_FALLING,"irqname", NULL) to prepare the ISR.
In cosmo_gpio_uart_recv_irq(), only record the irq count.
static irqreturn_t cosmo_gpio_uart_recv_irq(int irq, void *dev_id)
{
   irq_counts++;
  return IRQ_HANDLED;
}
I found if the GPIO5_13 triggers a very frequent falling_edge (for example, total 5 falling_edge, 200us between two falling_edge) ,
The ISR will miss 2 interrupt , the irq_counts is only 3.
if I pull another GPIO to measure it with oscilloscope as below:
int bb=0;
static irqreturn_t cosmo_gpio_uart_recv_irq(int irq, void *dev_id)
{
    irq_counts++;
   gpiod_set_value(gpio_dev->gpiod2,bb);
   bb=!bb;
  return IRQ_HANDLED;
}
in oscilloscope ,it shows the latency between real hardware interrupt and gpiod_set_value() is about 380us.
380 microseconds is the expected value?
How can I optimize to decrease the latency?
I hope to record the counts of square wave whose period time is 200us in this pin.
Thanks
Hi @imx8-mdt,