weston

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

weston

1,669件の閲覧回数
gopal_rhsharma
Contributor I

Hi,

We r using Gui-guider application and need to run separate DMS app with size 160x160. we need to fix DMS APP position on window and run always top of the Gui-guider running app how it possible please Suggest or help.

working setup is:-

imx93evk-11x11

DISTRO=fsl-imx-xwayland MACHINE=imx93evk source imx-setup-release.sh -b build-xwayland

BSP 6.6.3

weston 12.0.3

Thanks

0 件の賞賛
返信
2 返答(返信)

1,649件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If you are working with LVGL you can configure the GUI at the position you want. please open the source code of the GUI.

Regards

0 件の賞賛
返信

1,639件の閲覧回数
gopal_rhsharma
Contributor I
Hi,
LVGL GUI configured at the position but we need to run 2nd application top of GUI LVGL application. 2nd app streaming the video by gstemer. but every new start it position change. we required to freeze the position of streaming on top of running LVGL Application.
0 件の賞賛
返信