vpu encoding/decoding parallely

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

vpu encoding/decoding parallely

4,540 Views
gautammanam
Contributor I

HI,

I am trying to encode camera buffers to H264 and stream the rtp packets and at same time i am recieving the H264 rtp packets and decoding it. I am using VPU through openmax layer for encoding and decoding .


Stream is 720P and at 15 FPS it works fine, but at 25fps i see decoding becomes slow. And CPU usage becomes 80-90% .  As per documents VPU is capable of decoding 60 FPS

Any suggestions where to look into the issue. Does imx6 capable of 720P video conferencing ?

0 Kudos
Reply
3 Replies

3,210 Views
igorpadykov
NXP Employee
NXP Employee

Hi GAUTAM

one can look at presentation below p.6 it shows multistream performance:

2 simultaneous instances of 720p@30fps encode/decode, so seems for

encode+decode more realistic is 30fps

Q&A: MX6 VPU H.264 Dual Stream Encode Limits

For increasing vpu performance one can increase vpu frequency up to 352MHz,

Disable DFVS

echo performance > sys/devices/system/cpu/cpu0/cpufreq/scaling_governor

some suggestions can found below

GStreamer i.MX6 Multi-Overlay

for testing it is recommended to use imx-test/ mxc_vpu_test, included in BSP:

L3.14.28_1.0.0_iMX6QDLS_BUNDLE

http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,210 Views
gautammanam
Contributor I

Hi Igor,

When doing encoding/decoding simultaneously, i am getting around 30fps total for 720P H264 encode+decode. [15pfs for decoding and 15 fps for encoding] .

This is way less when compared to the above mentioned document. I can see i am getting enough rtp packets from network, but vpu decoder is slow in decoding  .And i am using VPU through fsl_imx_omx layer.  I am not sure if i am missing some thing. Can you suggest any VPU settings that i am missing.

IMX6Q sabre-Lite board

kernel 3.0.35

0 Kudos
Reply

3,210 Views
igorpadykov
NXP Employee
NXP Employee

Hi GAUTAM

these figures are given for vpu standalone performance, that is without

additional applications (which may consume bandwidth) like rtp network,

please try with unit-test (imx-test) mxc_vpu_test

Index of /buildsources/i/imx-test/imx-test-3.14.28-1.0.0

Best regards

igor

0 Kudos
Reply