vpu decoder error Got not enough input message

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

vpu decoder error Got not enough input message

2,769件の閲覧回数
rohanbaid
Contributor I

Please help what can be reason for the vpudec error : Got not enough input message

on IM6x .

0 件の賞賛
返信
4 返答(返信)

2,455件の閲覧回数
saurabh206
Senior Contributor III

Hi Rohan,

Can you provide more detail about what hardware you are using and what is your BSP?

Can you provide log message?

Saurabh

0 件の賞賛
返信

2,455件の閲覧回数
rohanbaid
Contributor I

I am using IM6x Sabrelte board. About which BSP i'm not sure how to answer that all i can give you the info is

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35-2508-g54750ff

   Image Type:   ARM Linux Kernel Image (uncompressed)

and the error log looks like something below:

PFW_FS::pfw_fs_play_file::387::Play File Path: /mnt/my_work/58f_6387_JLLJ3YQ6/H264_test5_voice_mp4_480x360.mp4

LOG_MP::gstreamer_flushMetadata::15975::psMetadata = 15211344

Qt::rg_open_metadata_files::1984:: no Entries .... Exiting

QML:: index at 0

-sh: r: command not found

root@freescale ~$ [INFO]        Product Info: i.MX6Q/D/S

vpudec versions :smileyhappy:

        plugin: 3.0.7

        wrapper: 1.0.35(VPUWRAPPER_ARM_LINUX Build on Mar 20 2015 11:55:21)

        vpulib: 5.4.12

        firmware: 2.1.9.36350

[INFO]  bitstreamMode 1, chromaInterleave 1, mapType 0, tiled2LinearEnable 0

LOG_MP::gstreamer_create_filesrc_video_pipeline::5023:: Audio Codec and Video codec is notavailable for given File So Exiting

LOG_MP::my_work_mp_open::16886::Could not create new pipeline

LOG_MP::my_work_mp_open::18568::Error, Leaving gstreamer_open

PFW_FS::pfw_fs_play_device::592::ERROR:: pfw_fs_play_file failed. Will process for Next-Track. Error: 0X409

root@freescale ~$ [INFO]        Product Info: i.MX6Q/D/S

vpudec versions :smileyhappy:

        plugin: 3.0.7

        wrapper: 1.0.35(VPUWRAPPER_ARM_LINUX Build on Mar 20 2015 11:55:21)

        vpulib: 5.4.12

        firmware: 2.1.9.36350

[INFO]  bitstreamMode 1, chromaInterleave 1, mapType 0, tiled2LinearEnable 0

LOG_MP::gstreamer_create_filesrc_video_pipeline::5023:: Audio Codec and Video codec is notavailable for given File So Exiting

LOG_MP::my_work_mp_open::16886::Could not create new pipeline

LOG_MP::my_work_mp_open::18568::Error, Leaving gstreamer_open

PFW_FS::pfw_fs_play_track_control::1006::ERROR:: fp_play_filefailed. Error: 0X409

PFW_FS::pfw_fs_play_device::546::ERROR:: pfw_fs_play_track_control failed. Error: 0X409

Qt::rg_play_device::263::failed in play device

Qt::rg_play_device::264::uistatus = 1033

Qt::rg_gui_remove_rows::2117::No Entries in listmodel, so ignoring the event count = 0

Qt::rg_open_metadata_files::1984:: no Entries .... Exiting

QML:: index at 0

Qt::rg_gui_remove_rows::2117::No Entries in listmodel, so ignoring the event count = 0

Qt::rg_open_metadata_files::1984:: no Entries .... Exiting

QML:: index at 0

The error from vpudec is

0:00:03.408820045  [334m 2715 [00m   0xe51ab8  [31;01mERROR   [00m  [00m          vpudec vpudec.c:1498:gst_vpudec_chain: [00m Func VPU_DecDecodeBuf failed!! with ret 1

0:00:03.408979909  [334m 2715 [00m   0xe51ab8  [33;01mWARN    [00m  [00m          vpudec vpudec.c:1409:gst_vpudec_process_error:<vpudec0> [00m error: unknown error detect

and for every vpudec chain I get

0:00:03.406773909  [334m 2715 [00m   0xe51ab8  [32;01mINFO    [00m  [00m          vpudec vpudec.c:1588:gst_vpudec_chain: [00m Got not enough input message!!

I dont know why this occurs but itseems that before getting this issue I have already pushed 20 seconds worth of data.

0 件の賞賛
返信

2,455件の閲覧回数
rohanbaid
Contributor I

Hi,

          In the link https://community.freescale.com/thread/311316#348520 , Kuniakic Chiba san speaks about making a single mp4 file work on im6x with qtdemux and vpudec. I tried the same thing but it did not work.

     So please suggest any remedy or anything to try out to find out the bug more precisely.

0 件の賞賛
返信

2,455件の閲覧回数
rohanbaid
Contributor I

Sorry about the above mail tried correctly and the above thing worked.

Thank You

0 件の賞賛
返信