viv_samples UnitTests execute failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

viv_samples UnitTests execute failed

2,147件の閲覧回数
wei-fonglin
Contributor II

Hi All,

We made a custom i.MX6q board. The BSP version is imx-3.10.53-1.1.2_patch.

We executed the test applications in /opt/viv_samples/cl11/UnitTest/test_vivante

and found functions_and_kernels 、multi_dimensional_arrays、initializers and structs_and_enums were failed to pass.

But if we recompile the os with imx-gpu-viv version imx-gpu-viv_5.0.11.p4.1-hfp, these test applications passed.

Due to customer's spec, we have to use imx-gpu-viv version imx-gpu-viv_5.0.11.p4.3-hfp.

Is there any way to solve these problems in version 5.0.11.p4.3? Thanks.

Original Attachment has been moved to: structs_and_enums.log.zip

Original Attachment has been moved to: functions_and_kernels.log.zip

Original Attachment has been moved to: initializers.log.zip

Original Attachment has been moved to: multi_dimensional_arrays.log.zip

ラベル(5)
0 件の賞賛
返信
2 返答(返信)

1,940件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Wei-Fong,

You should give a try to the latest  imx-gpu-viv-5.0.11.p4.5

Hope it helps

0 件の賞賛
返信

1,940件の閲覧回数
wei-fonglin
Contributor II

Hi Bio_TICFSL,

Thanks for reply.

I tried imx-gpu-viv-5.0.11.p4.5 today but had the same situation.

Do you find the same problem in sabresd or any development board ?

Because I want to know if this is caused by our wrong settings or any other reason.

Thanks.

0 件の賞賛
返信