v4l2 capture

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

v4l2 capture

3,823件の閲覧回数
MatthiasFend
Contributor I

hi,

 

I just tried to get the CSI interface of the 53QSB to work:

 

First I load the modules:

> modprobe mxc_v4l2_capture

> modprobe ov3640_camera

 

But when I try to access these driver with the supplied test utilities

(mxc_v4l2_overlay.out, mxc_v4l2_capture.out) I always get error messages like these:

ERROR: v4l2 capture: slave not found!
Unable to open /dev/video0

 

I figured out that the probe method of the ov3640 is also not called (after modprobe).

 

For the test I used L2.6.35_11.01.00_ER.

When I use the same kernel&rootfs with the IMX51EVK everything works well.

So I guess it's something board/processor specific.

 

Any hints?

 

Thanks,

 Matthias

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,851件の閲覧回数
MatthiasFend
Contributor I

sorry for the late reply - probaply i missed some notifiers...

i was editing mx53_evk board file, but of course the mx53_loco is the file which is used on the QSB.

so i changed something and, of course, nothing happend...

~matthias

0 件の賞賛
返信

2,851件の閲覧回数
DualDisplayiss1
Contributor I


Hi~~Matthias:

i also meet this problem when i change ov3640 to adv7180.

 

what do you mean >caught by the "naming" trap.

 

can you describe more.

 

 

thanks

Eric

 

shricco said:

Hi Matthias,

I am facing the same problem with the unable to open /dev/video0.

 

What exactly have you done to get it working? I tried running the unit tests on the ubuntu 10.04 shipped with my i.mx53 QSB.

 

Thx in advance

 

Chris


Matthias Fend said:

arggh. evk,qsb,loco, ...  caught by the "naming" trap.

mx53_loco is the place to be (not mx53_evk).

 

thanks,

 ~matthias

 

0 件の賞賛
返信

2,851件の閲覧回数
shricco
Contributor I

Hi Matthias,

I am facing the same problem with the unable to open /dev/video0.

 

What exactly have you done to get it working? I tried running the unit tests on the ubuntu 10.04 shipped with my i.mx53 QSB.

 

Thx in advance

 

Chris


Matthias Fend said:

arggh. evk,qsb,loco, ...  caught by the "naming" trap.

mx53_loco is the place to be (not mx53_evk).

 

thanks,

 ~matthias

 

0 件の賞賛
返信

2,851件の閲覧回数
MatthiasFend
Contributor I

arggh. evk,qsb,loco, ...  caught by the "naming" trap.

mx53_loco is the place to be (not mx53_evk).

 

thanks,

 ~matthias

0 件の賞賛
返信