uuu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
3,730 Views
tgt007
Contributor II

I had an error while upgrading mcimx93.As shown in attachment.Can you see what's going on?There is no problem with the imx8mm upgrade.

bb.jpguuu.jpg

Tags (1)
0 Kudos
Reply
1 Solution
3,665 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Latest images are not supported on A0 silicon revision, the latest working release on that silicon revision is Linux 6.1.22_2.0.0.

Best regards.

View solution in original post

0 Kudos
Reply
5 Replies
3,707 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Could you please help me with the next information?

- i.MX93 silicon revision.

- Linux version.

Best regards.

0 Kudos
Reply
3,688 Views
tgt007
Contributor II

U-Boot 2023.04-lf_v2023.04+gaf7d004eaf (Jun 06 2023 - 14:59:40 +0000)

CPU: i.MX93(52) rev1.0 1700 MHz (running at 1692 MHz)
CPU: Consumer temperature grade (0C to 95C) at 36C
Reset cause: POR (0x1)
Model: NXP i.MX93 11X11 EVK board
DRAM: 1.7 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C2 0x52]









LF_v6.6.3-1.0.0_images_IMX93EVK


0 Kudos
Reply
3,685 Views
tgt007
Contributor II

tgt007_0-1715307507329.jpeg

tgt007_1-1715307534745.jpeg

 

 

0 Kudos
Reply
3,666 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Latest images are not supported on A0 silicon revision, the latest working release on that silicon revision is Linux 6.1.22_2.0.0.

Best regards.

0 Kudos
Reply
3,649 Views
tgt007
Contributor II
Do you have an old version of the user manual?
0 Kudos
Reply