use of aes-128,sha-256 algorithms

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

use of aes-128,sha-256 algorithms

1,264件の閲覧回数
manivannanm
Contributor I

hi all,

     im new to free scale. i found out that mx6 supports aes-128/256 , sha-256 algorithms. But i dont knw how it works. please anyone help me with this..

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,121件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Manivannan

first please obtain copy Security Reference Manual for i.MX 6

IMX6DQ6SDLSRM

Software usage is described in

i.MX_6_Linux_Reference_Manual.pdf

Chapter 51 CAAM (Cryptographic Acceleration and Assurance Module)

included in doc bundle below

L3.10.17_1.0.0_LINUX_DOCS Linux 3.10.17 BSP & MM Bundle

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信