use SPI MCP23S17

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

use SPI MCP23S17

跳至解决方案
7,959 次查看
tobias_mrs
Contributor III

Hello
I have problems to get the GPIO Port Expander MCP23S17 to run and to use the Driver gpio-mcp23s08.c on a i.MX6


I have add the following Kernel configs

 CONFIG_GPIO_MCP23S08=y
CONFIG_SPI_IMX=y

I have change my Devicetree like following:

&ecspi1 {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_ecspi1>;
    fsl,spi-num-chipselects = <2>;
    cs-gpios = <
        &gpio2 30 GPIO_ACTIVE_HIGH
        &gpio3 19 GPIO_ACTIVE_HIGH
    >;
    status = "okay";

    gpiom0: gpio8@0 {
        compatible = "microchip,mcp23s17";
        gpio-controller;
        #gpio-cells = <2>;
        microchip,spi-present-mask = <0x01>;
        reg = <0>;
        spi-max-frequency = <1000000>;
        };

    spidev1: spi@1 {
        compatible = "spidev";
        reg = <1>;
        spi-max-frequency = <54000000>;
    };
};

With

dmesg | grep spi
I get

[ 3.751757] spi_imx 2008000.ecspi: registered master spi0
[ 3.756600] spi spi0.0: spi_imx_setup: mode 0, 8 bpw, 1000000 hz
[ 3.761616] spi spi0.0: setup mode 0, 8 bits/w, 1000000 Hz max --> 0
[ 3.770168] spi_imx 2008000.ecspi: registered child spi0.0
[ 3.780987] spi spi0.1: spi_imx_setup: mode 0, 8 bpw, 54000000 hz
[ 3.785848] spi spi0.1: setup mode 0, 8 bits/w, 54000000 Hz max --> 0

How do I load, test and use the gpio-mcp23s08 Driver?

regards

Tobias

标签 (2)
0 项奖励
回复
1 解答
6,768 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Tobias

control registers of MCP23S17 should be programmed appropriately, please

check examples on

https://www.raspberrypi.org/forums/viewtopic.php?t=5987
http://www.retrosemi.co.uk/mcp23s17/Getting_started_with_the_mcp23s17.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
6,768 次查看
tobias_mrs
Contributor III

Hello

thanks for the examples.
I have now finished the experiment with the Decivetree, I don't get it run.

I have now implement my own control for the mcp23s17 like the example.
But now I get on every transfer on the spi bus the following message:

mx51_ecspi_clkdiv: fin: 60000000, fspi: 50000000, post: 0, pre: 1

Whats wrong now?

regards

Tobias

0 项奖励
回复
6,768 次查看
igorpadykov
NXP Employee
NXP Employee

seems ratio between fin, fspi should be integer, please look at

Figure 18-1 i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards
igor

0 项奖励
回复
6,768 次查看
tobias_mrs
Contributor III

Hello
thanks for the answer

the Problem was that I have enabled the DEBUG messages from the kernel and the the driver spi-imx.c allays displays its frequency.

function: mx51_ecspi_clkdiv:
    pr_debug("%s: fin: %u, fspi: %u, post: %u, pre: %u\n",  __func__, fin, fspi, post, pre);

Best regards

Tobias

0 项奖励
回复
6,769 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Tobias

control registers of MCP23S17 should be programmed appropriately, please

check examples on

https://www.raspberrypi.org/forums/viewtopic.php?t=5987
http://www.retrosemi.co.uk/mcp23s17/Getting_started_with_the_mcp23s17.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复