usb problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb problem

1,021 Views
eao
Contributor I

Hello, I would like to ask a question, in the official example of usb, "dev_cdc_vcom_bm_cm7" is used as a slave device and the computer is used as the master device to send data to the development board, I found that multiple interrupts are generated and each interrupt has 512 bytes, is there an example of this? Is there any example where only one interrupt can be generated and all data will be received? Thanks!

Labels (1)
0 Kudos
Reply
0 Replies