usb mass storage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb mass storage

Jump to solution
4,461 Views
yan2anfei
Contributor III

hi ,

I have a imx6slevk board, which use the linux  4.1.15.

I wan't to achive the function when pc connect the board through usb, a usb mass storage device is appear. 

thanks a lot.

Labels (2)
1 Solution
3,587 Views
igorpadykov
NXP Employee
NXP Employee

Hi yan2

please follow steps to enable mass storage as gadget driver

in attached Linux Manual sect.39.2.9 USB OTG and unit tests

imx-test (../mxc_usb_test)
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
3,588 Views
igorpadykov
NXP Employee
NXP Employee

Hi yan2

please follow steps to enable mass storage as gadget driver

in attached Linux Manual sect.39.2.9 USB OTG and unit tests

imx-test (../mxc_usb_test)
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------