usb ethernet for i.mx6 in u-boot level with u-boot_201304

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usb ethernet for i.mx6 in u-boot level with u-boot_201304

2,244件の閲覧回数
宗標廖
Contributor V

Hello,Community.

I want to add USB ethernet(convert USB to ethernet) function in u-boot level with u-boot_201304 for i.MX6.

Could someone tell me how to achieve it?

Thank you!

Best Regards,

ZongbiaoLiao

ラベル(3)
タグ(4)
2 返答(返信)

1,476件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

suggest to look at Nitrogen uboot as it impelmented USB network

protocol

http://boundarydevices.com/u-boot-2014-01/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,476件の閲覧回数
宗標廖
Contributor V

Hello,

If someone has the same requirement with me,Please refer to <u-boot_201304>/doc/README.usb.