usb ethernet for i.mx6 in u-boot level with u-boot_201304

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb ethernet for i.mx6 in u-boot level with u-boot_201304

2,053 Views
宗標廖
Contributor V

Hello,Community.

I want to add USB ethernet(convert USB to ethernet) function in u-boot level with u-boot_201304 for i.MX6.

Could someone tell me how to achieve it?

Thank you!

Best Regards,

ZongbiaoLiao

Labels (3)
2 Replies

1,285 Views
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

suggest to look at Nitrogen uboot as it impelmented USB network

protocol

http://boundarydevices.com/u-boot-2014-01/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,285 Views
宗標廖
Contributor V

Hello,

If someone has the same requirement with me,Please refer to <u-boot_201304>/doc/README.usb.