usb cdc-acm error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usb cdc-acm error

5,731件の閲覧回数
jjysekm
Contributor I

Dear NXP Team,

We are currently using L4.14.98 release we are observing error relating usb cdc-acm in imx8dx

[xhci-cdns3: WARN urb submitted to disabled ep
cdc_acm 1-1:1.2: acm_port_activate - usb_submit_urb(ctrl irq) failed
xhci-cdns3: WARN urb submitted to disabled ep
cdc_acm 1-1:1.2: acm_port_activate - usb_submit_urb(ctrl irq) failed

[..]

cdc_acm 1-1:1.0: failed to set dtr/rts
xhci-cdns3: ERROR unknown endpoint state for ep
cdc_acm 1-1:1.1: urb 2 failed submission with -22
xhci-cdns3: ERROR unknown event type 31
xhci-cdns3: ERROR unknown event type 22
xhci-cdns3: WARN waiting for error on ep to be cleared
cdc_acm 1-1:1.0: failed to set dtr/rts
xhci-cdns3: ERROR unknown endpoint state for ep
cdc_acm 1-1:1.3: acm_start_wb - usb_submit_urb(write bulk) failed: -22
systemd: 20 output lines suppressed due to ratelimiting

Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000008b

Why this error is observed?

How to resolve this error?

0 件の賞賛
返信
2 返答(返信)

5,248件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Joys,

I’m afraid that i.MX8DX family is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信

5,248件の閲覧回数
Raana
Contributor III

Hi Carlos,

Even I'm also facing the same issue with the same source but on i.Mx8qxp.

We are connecting LTE module through USB. There, I'm getting the below error while power OFF and ON the module.

"cdc_acm 1-1:1.0: failed to set dtr/rts"


Can you help me to resolve this?

Thank You.

Best Regards,

J.P.Raja

0 件の賞賛
返信