Dear team,
My customer found the following description on your i.MX6Solo/DualLite/Datasheet(IMX6SDLCEC,Rev.9).
“VDD_SOC LDO output set point is equal to the VDD_PU LDO output set point.”
The VDD_PU is the power for graphics feature and they do not use it, then they use the VDD_PU_CAP outputs voltages is about 0.15V and VDD_SOC and VDD_PU is differ.
Is it possible to use VDD_PU as like this even Graphic feature is not used?
Best Regards,
Miyamoto
Hello,
According to the Datasheet VDD_SOC LDO output set point must be set equal to
the VDD_PU LDO output set point (in LDO enabled mode) without any relation whether
GPU is used or not.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.