unable to connect wire for probe index 1 in while debuggine mimxrt1170

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

unable to connect wire for probe index 1 in while debuggine mimxrt1170

跳至解决方案
1,244 次查看
sandeep_c
Contributor I

unable to connect wire for probe index 1 in while debuggine mimxrt1170

iam getting the above error while debgging the rt1170evk board

i_MXRT1170Processor_0-1675322140714.png

 

0 项奖励
回复
1 解答
1,230 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I recommend reviewing the information on the page for the first use. Maybe need the external DC, it does not have an external DC please modify the power selection jumper or the boot source switch is wrong. The next link show, which is the USB for debugging, or if you are using an external debugger need an adapter to connect un the JTAG [J1].

Getting Started with the i.MX RT1170 Evaluation Kit | NXP Semiconductors

Best regards,
Pavel

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,231 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I recommend reviewing the information on the page for the first use. Maybe need the external DC, it does not have an external DC please modify the power selection jumper or the boot source switch is wrong. The next link show, which is the USB for debugging, or if you are using an external debugger need an adapter to connect un the JTAG [J1].

Getting Started with the i.MX RT1170 Evaluation Kit | NXP Semiconductors

Best regards,
Pavel

0 项奖励
回复
1,226 次查看
sandeep_c
Contributor I
i boot the the rt1170 its working fine thanks for the reply
0 项奖励
回复