unable to connect wire for probe index 1 in while debuggine mimxrt1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

unable to connect wire for probe index 1 in while debuggine mimxrt1170

Jump to solution
1,203 Views
sandeep_c
Contributor I

unable to connect wire for probe index 1 in while debuggine mimxrt1170

iam getting the above error while debgging the rt1170evk board

i_MXRT1170Processor_0-1675322140714.png

 

0 Kudos
Reply
1 Solution
1,189 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I recommend reviewing the information on the page for the first use. Maybe need the external DC, it does not have an external DC please modify the power selection jumper or the boot source switch is wrong. The next link show, which is the USB for debugging, or if you are using an external debugger need an adapter to connect un the JTAG [J1].

Getting Started with the i.MX RT1170 Evaluation Kit | NXP Semiconductors

Best regards,
Pavel

View solution in original post

0 Kudos
Reply
2 Replies
1,190 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I recommend reviewing the information on the page for the first use. Maybe need the external DC, it does not have an external DC please modify the power selection jumper or the boot source switch is wrong. The next link show, which is the USB for debugging, or if you are using an external debugger need an adapter to connect un the JTAG [J1].

Getting Started with the i.MX RT1170 Evaluation Kit | NXP Semiconductors

Best regards,
Pavel

0 Kudos
Reply
1,185 Views
sandeep_c
Contributor I
i boot the the rt1170 its working fine thanks for the reply
0 Kudos
Reply